AttributeTemplatesBuilderConstraintOptions Enumeration¶
NXOpen.AttributeTemplatesBuilder.ConstraintOptions is an alias for NXOpen.AttributeTemplatesBuilderConstraintOptions
-
class
NXOpen.
AttributeTemplatesBuilderConstraintOptions
¶ Bases:
object
Specifies the constraint data associated with the template. All constraints are enabled for templates of type integer, number, string, and date.
Enum Members
Enum Member Enum Member Description NotSet No constraint data, no further action is needed UpperLimit This template has an upper limit but no lower limit. The max value must be set. Available for integer, number, string, and date types. LowerLimit This template has a lower limit but no upper limit. The min value must be set. Available for integer, number, string, and date types. UpperAndLowerLimit This template has a lower limit and an upper limit. The min and max must also be set. Available for integer, number, string, and date types. List List of values, the value list must also be set. Only available for integer, number, and string types. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-