AttributePropertiesBaseBuilderObjectOptions Enumeration¶
NXOpen.AttributePropertiesBaseBuilder.ObjectOptions is an alias for NXOpen.AttributePropertiesBaseBuilderObjectOptions
-
class
NXOpen.
AttributePropertiesBaseBuilderObjectOptions
¶ Bases:
object
Specifies which object will be used when applying attributes. The options available are determined by the objects passed in. These options will not be used if the object passed in is a part.
Deprecated since version NX8.5.0: Use
NXOpen.AttributePropertiesBaseBuilder.SetAttributeObjects()
instead.Enum Members
Enum Member Enum Member Description Object Apply attribute to the object in the select object list Feature Apply attribute to the feature in the select object list Occurrence Apply attribute to the occurrence only ComponentInstance Apply attribute to the instance of the component. All occurrences of the instance will inherit this attribute. ReferenceSet Apply attribute to the reference set ObjectInComponentPart Apply attribute to the object in the component part ComponentAsPartAttribute Apply attribute to the component as a part attribute Empty No objects are contained in the select object list -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-