AttributePropertiesBaseBuilderDataTypeOptions Enumeration¶
NXOpen.AttributePropertiesBaseBuilder.DataTypeOptions is an alias for NXOpen.AttributePropertiesBaseBuilderDataTypeOptions
-
class
NXOpen.
AttributePropertiesBaseBuilderDataTypeOptions
¶ Bases:
object
Specifies the data type of the attribute, this cannot be changed once the attribute has been created
Enum Members
Enum Member Enum Member Description Null Null, the attribute will have no value Boolean Boolean, the value will be true or false Integer Integer, the value is a whole number Number Number, the value is a floating point number and may contain units String String, the value will be a textual string Date Date, the value will be date and time -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-