AbsolutePositionBuilder Class |
Represents a builder class that absolutely positions the specified objects. |
AddComponentBuilder Class |
Represents a builder class that performs add existing component operation in current context. |
Arrangement Class |
Manages the suppression of NXOpen.Assemblies.Component`s within a :py:class:`NXOpen.Assemblies.ComponentAssembly . |
ArrangementCollection Class |
a collection of arrangements |
ArrangementsBuilder Class |
Represents an arrangements builder that selects an arrangement |
AssembliesGeneralPropertiesBuilder Class |
Represents an NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder to be used for changing the general properties of a component. |
AssembliesParameterPropertiesBuilder Class |
Represents an NXOpen.Assemblies.AssembliesParameterPropertiesBuilder to be used for changing the name or modifying the positioning mixture status of a component. |
Assembly Class |
Assembly class |
AssemblyManager Class |
Represents the Assembly Manager |
AttributeSearchTerm Class |
An attribute search term within a NXOpen.Assemblies.SubsetRecipe . |
AttributeSearchTermBuilder Class |
An AttributeSearchTermBuilder is used to create or edit an NXOpen.Assemblies.AttributeSearchTerm . |
BoxSearchTerm Class |
A volume search term within a NXOpen.Assemblies.SubsetRecipe . |
BoxSearchTermBuilder Class |
A BoxSearchTermBuilder is used to create or edit an NXOpen.Assemblies.BoxSearchTerm . |
ClearanceAnalysisBuilder Class |
Represents NXOpen.Assemblies.ClearanceAnalysisBuilder . |
ClearanceSet Class |
Represents NXOpen.Assemblies.ClearanceSet . |
ClearanceSetCollection Class |
Represents NXOpen.Assemblies.ClearanceSetCollection . |
Component Class |
Represents a component in a NXOpen.Assemblies.ComponentAssembly . |
ComponentAssembly Class |
Represents the set of :py:class:`NXOpen.Assemblies.Component`s that make up an assembly. |
ComponentGroup Class |
Represents a Component Group that is defined within an Assembly. |
ComponentGroupCollection Class |
|
ComponentOrder Class |
Represents an order object that stores the order of child NXOpen.Assemblies.Component`s in context of parent :py:class:`NXOpen.Assemblies.ComponentAssembly . |
ComponentPattern Class |
Represents the component pattern class. |
ComponentPatternBuilder Class |
Represents a builder class that performs various NXOpen.Assemblies.ComponentPattern operations. |
ComponentPatternCollection Class |
Represents the collection object for all component patterns. |
ConstraintDisplayBuilder Class |
The NXOpen.Assemblies.ConstraintDisplayBuilder can be used to control visibility of constraints and optionally components. |
CopyDesignElementBuilder Class |
Represents a builder class that performs copying design element operation in 4GD. |
CreateComponentBuilder Class |
Represents a NXOpen.Assemblies.CreateComponentBuilder builder class. |
CreateNewComponentBuilder Class |
Represents a NXOpen.Assemblies.CreateNewComponentBuilder builder class. |
CreateOverridePartBuilder Class |
Represents a builder class that creates empty override part in the specified design elements. |
DeleteOverridePartBuilder Class |
Represents a builder class that deletes override part in the specified design elements. |
DesignElementBuilder Class |
Represents a builder class that performs various design element operations. |
DrawingExplosion Class |
Represents an explosion used in a drawing view of an arrangement. |
DrawingExplosionCollection Class |
Represents a collection of drawing explosions |
ExplicitSearchTerm Class |
A NXOpen.Assemblies.SubsetRecipe search term that refers explicitly to a design element. |
ExplodedComponent Class |
Represents a NXOpen.Assemblies.Component within an explosion. |
Explosion Class |
Represents an explosion. |
ExplosionCollection Class |
Represents a collection of explosions |
FindInCollaborativeDesign Class |
FindInCollaborativeDesign is a searcher for performing simple searches in the context of a subset. |
GroupSearchTerm Class |
A group of NXOpen.Assemblies.SearchTerm`s within a :py:class:`NXOpen.Assemblies.SubsetRecipe . |
HideComponentBuilder Class |
Represents a NXOpen.Assemblies.HideComponentBuilder |
LoadInterpartDataBuilder Class |
Represents a builder:py:class:NXOpen.Assemblies.LoadInterpartDataBuilder |
MakeUniquePartBuilder Class |
Represents a NXOpen.Assemblies.MakeUniquePartBuilder builder. |
MechanicalRoutingSubsetBuilder Class |
A MechanicalRoutingSubsetBuilder is used to create/edit Subsets NXOpen.Assemblies.Subset that are used to define the context needed to perform a Mechanical Routing Design activity. |
Order Class |
Represents base class for all Order classes. |
OrderCollection Class |
a collection of :py:class:`NXOpen.Assemblies.Order`s |
Partition Class |
A partition is a Teamcenter object in a Collaborative Design. |
PartitionList Class |
Represents a list of objects. |
PartitionScheme Class |
A partition scheme is a Teamcenter object in a Collaborative Design. |
PartitionSearchTerm Class |
A Assemblies.SubsetRecipe search term that refers to a partition. |
PatternInstance Class |
Represents the pattern instance object. |
PatternMaster Class |
Represents the pattern master object. |
PatternMember Class |
Represents the pattern member object. |
PlaneSearchTerm Class |
A plane search term within a NXOpen.Assemblies.SubsetRecipe . |
PlaneSearchTermBuilder Class |
A PlaneSearchTermBuilder is used to create or edit an NXOpen.Assemblies.PlaneSearchTerm . |
PositioningGroup Class |
Represents the class for positioning group. |
PositioningGroupBuilder Class |
Represents builder class for positioning group which is used to store constraints for design element. |
PositioningTask Class |
Represents the class for positioning task. |
PositioningTaskBuilder Class |
Represents the class for positioning task builder |
ProductOutlineBuilder Class |
Represents a builder NXOpen.Assemblies.ProductOutlineBuilder . |
ProductOutlineManager Class |
Represents a collection of assemblies. |
ProximitySearchTerm Class |
A proximity search term within a NXOpen.Assemblies.SubsetRecipe . |
ProximitySearchTermBuilder Class |
A ProximitySearchTermBuilder is used to create or edit an Assemblies.BoxSearchTerm . |
RelinkerBuilder Class |
Represents a NXOpen.Assemblies.RelinkerBuilder |
RelinkerCollection Class |
Represents a collection of relinker |
ReplaceComponentBuilder Class |
Represents a NXOpen.Assemblies.ReplaceComponentBuilder builder. |
RunContentProximitySearchTerm Class |
A proximity search term within a NXOpen.Assemblies.SubsetRecipe . |
RunContentProximitySearchTermBuilder Class |
A RunContentProximitySearchTermBuilder is used to create or edit an Assemblies.RunContentProximitySearchTerm . |
SearchResultCollection Class |
A collection of :py:class:`NXOpen.Assemblies.SearchResultElement`s. |
SearchResultElement Class |
A search result element can be produced as the result of a search performed in the context of a NXOpen.Assemblies.SubsetBuilder . |
SearchTerm Class |
A search term is used to specify a search for the contents of a NXOpen.Assemblies.Subset . |
SearchTermBuilder Class |
A SearchTermBuilder is used to create or edit an NXOpen.Assemblies.SearchTerm . |
SelectComponent Class |
Represents a single object selection. |
SelectComponentList Class |
Represents a list of objects on a selection list. |
ShowComponentBuilder Class |
Represents a NXOpen.Assemblies.ShowComponentBuilder |
Subset Class |
A subset is a set of design elements within a collaborative design. |
SubsetBuilder Class |
A SubsetBuilder is used to create or edit an NXOpen.Assemblies.Subset . |
SubsetCollection Class |
Represents a collection of subset. |
SubsetConfigurationBuilder Class |
A SubsetConfigurationBuilder is used to edit the revision rule and effectivity used to configure the contents of the subset. |
SubsetRecipe Class |
A subset recipe is used by a NXOpen.Assemblies.SubsetBuilder to collect :py:class:`NXOpen.Assemblies.SearchTerm`s. |
UpdateDesignElementPositionBuilder Class |
Represents the builder class that updates positions of the DE’s(Shape/Reuse) or Subordinates with override that are out of date. |
UpdateStructureBuilder Class |
Represents a builder NXOpen.Assemblies.UpdateStructureBuilder . |
WaveQuery Class |
Provides information about the inter-part relations (e.g. WAVE, inter-part expressions) in a NX model. |