SearchResultCollection Class¶
-
class
NXOpen.Assemblies.
SearchResultCollection
¶ Bases:
object
A collection of :py:class:`NXOpen.Assemblies.SearchResultElement`s.
To obtain an instance of this class, refer to
NXOpen.Assemblies.SubsetBuilder
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Assemblies.SearchResultElement with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
SearchResultCollection.
FindObject
¶ Finds the
NXOpen.Assemblies.SearchResultElement
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Name of the search result to be found Returns: Element found, or null if no such search result element exists. Return type: NXOpen.Assemblies.SearchResultElement
New in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)