ReplaceComponentBuilderComponentNameOption Enumeration¶
NXOpen.Assemblies.ReplaceComponentBuilder.ComponentNameOption is an alias for NXOpen.Assemblies.ReplaceComponentBuilderComponentNameOption
-
class
NXOpen.Assemblies.
ReplaceComponentBuilderComponentNameOption
¶ Bases:
object
Represents possible component name option for replace operation
Enum Members
Enum Member Enum Member Description Maintain Maintain the component name of the component being replaced out Original Use the replacement part name as the component name AsSpecified Set the specified component name -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-