ReplaceComponentBuilderComponentLayerOption Enumeration¶
NXOpen.Assemblies.ReplaceComponentBuilder.ComponentLayerOption is an alias for NXOpen.Assemblies.ReplaceComponentBuilderComponentLayerOption
-
class
NXOpen.Assemblies.
ReplaceComponentBuilderComponentLayerOption
¶ Bases:
object
Represents possible layer option for replacement part
Enum Members
Enum Member Enum Member Description Maintain Maintain the layer of the component being replaced out Original Set the layer to replacement part’s original layer Work Set the layer to current work layer AsSpecified Set the specified layer -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-