OrderCollection Class¶
-
class
NXOpen.Assemblies.
OrderCollection
¶ Bases:
object
a collection of :py:class:`NXOpen.Assemblies.Order`s
To obtain an instance of this class, refer to
NXOpen.Assemblies.ComponentAssembly
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Assemblies.Order with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
OrderCollection.
FindObject
¶ Finds the
NXOpen.Assemblies.Order
with the given identifier as recorded in a journal.This method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Name of the Order to be found Returns: Order found, or null if no such Order exists. Return type: NXOpen.Assemblies.Order
New in version NX9.0.0.
License requirements: None.