MechanicalRoutingSubsetBuilderSurroundingDataRecipeMethod Enumeration¶
NXOpen.Assemblies.MechanicalRoutingSubsetBuilder.SurroundingDataRecipeMethod is an alias for NXOpen.Assemblies.MechanicalRoutingSubsetBuilderSurroundingDataRecipeMethod
-
class
NXOpen.Assemblies.
MechanicalRoutingSubsetBuilderSurroundingDataRecipeMethod
¶ Bases:
object
Represents the method to use to determine the surrounding data corresponding to the routing design content that has been loaded. 1. None : No surrounding data to be loaded. 2. ProximityRoutingContent : This means surrounding data for the runs, this is related to the DE’s that are in proximity to the DEs constituting the run. 3. Manual: An empty Surrounding Object Subset will be created
Enum Members
Enum Member Enum Member Description NotSet ProximitytoRoutingContent Manual -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-