MakeUniquePartBuilderOption Enumeration

NXOpen.Assemblies.MakeUniquePartBuilder.Option is an alias for NXOpen.Assemblies.MakeUniquePartBuilderOption

class NXOpen.Assemblies.MakeUniquePartBuilderOption

Bases: object

Represents possible copy assembly options for unique part

Enum Members

Enum Member Enum Member Description
CopyAssemblyOnly
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.