LoadInterpartDataBuilderOpenUnloadedParentsType Enumeration¶
NXOpen.Assemblies.LoadInterpartDataBuilder.OpenUnloadedParentsType is an alias for NXOpen.Assemblies.LoadInterpartDataBuilderOpenUnloadedParentsType
-
class
NXOpen.Assemblies.
LoadInterpartDataBuilderOpenUnloadedParentsType
¶ Bases:
object
Represents the load interpart parent level types
Enum Members
Enum Member Enum Member Description NotSet Load all partially loaded parts that contain links and all immediate level parents parts if they are partially loaded ImmediateLevel Load all partially loaded parts that contain links and all immediate level parents parts regardless of load status AllLevels Load all partially loaded parts that contain links and all level parent parts regardless of load status -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-