ExplosionCollection Class¶
-
class
NXOpen.Assemblies.
ExplosionCollection
¶ Bases:
object
Represents a collection of explosions
To obtain an instance of this class, refer to
NXOpen.Assemblies.ComponentAssembly
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates an explosion based upon the default arrangement in the given OCC part. |
FindObject | Finds the NXOpen.Assemblies.Explosion with the given identifier as recorded in a journal. |
Method Detail¶
Create¶
-
ExplosionCollection.
Create
¶ Creates an explosion based upon the default arrangement in the given OCC part.
Signature
Create(explosionName)
Parameters: explosionName (str) – Name to be given to the new explosion Returns: the new explosion Return type: NXOpen.Assemblies.Explosion
New in version NX9.0.1.
License requirements: assemblies (“ASSEMBLIES MODULE”)
FindObject¶
-
ExplosionCollection.
FindObject
¶ Finds the
NXOpen.Assemblies.Explosion
with the given identifier as recorded in a journal.This method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(name)
Parameters: name (str) – Name of the Explosion to be found Returns: Explosion found, or null if no such Explosion exists. Return type: NXOpen.Assemblies.Explosion
New in version NX9.0.1.
License requirements: None.