DrawingExplosionCollection Class¶
-
class
NXOpen.Assemblies.
DrawingExplosionCollection
¶ Bases:
object
Represents a collection of drawing explosions
To obtain an instance of this class, refer to
NXOpen.Assemblies.ComponentAssembly
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Assemblies.DrawingExplosion with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
DrawingExplosionCollection.
FindObject
¶ Finds the
NXOpen.Assemblies.DrawingExplosion
with the given identifier as recorded in a journal.This method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(name)
Parameters: name (str) – Name of the DrawingExplosion to be found Returns: DrawingExplosion found, or null if no such DrawingExplosion exists. Return type: NXOpen.Assemblies.DrawingExplosion
New in version NX12.0.0.
License requirements: None.