DesignElementBuilderOperationType Enumeration¶
NXOpen.Assemblies.DesignElementBuilder.OperationType is an alias for NXOpen.Assemblies.DesignElementBuilderOperationType
-
class
NXOpen.Assemblies.
DesignElementBuilderOperationType
¶ Bases:
object
Represents an operation type that can be performed on a design element
Enum Members
Enum Member Enum Member Description Create Creates a design element Edit Edits a design element SaveAs Save as a design element Save Saves a design element SaveAndClose Saves a design element and if it is a reuse closes the reused part Undefined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-