DegreesOfFreedomStatus Enumeration¶
-
class
NXOpen.Assemblies.
DegreesOfFreedomStatus
¶ Bases:
object
The status of a rotation point, rotation axis or translation direction reported in
NXOpen.Assemblies.DegreesOfFreedom
. Enum MembersEnum Member Enum Member Description NotUsed The field is not used. Static The point or direction is well defined. Free The point or direction is under defined. Instantaneous The point or direction is instantaneous. StaticNormal The direction represents a normal to two translational degrees of freedom. The direction is well defined. FreeNormal The direction represents a normal to two translational degrees of freedom. The direction is under defined. InstantaneousNormal The direction represents a normal to two translational degrees of freedom. The direction is instantaneous. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-