DegreesOfFreedomResult Enumeration¶
-
class
NXOpen.Assemblies.
DegreesOfFreedomResult
¶ Bases:
object
The overall result of the degrees of freedom calculation reported in
NXOpen.Assemblies.DegreesOfFreedom
. Enum MembersEnum Member Enum Member Description Unknown The calculation failed to produce a result, possibly because the component is inconsistently constrained. Success The degrees of freedom calculation succeeded. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-