CreateNewComponentBuilderComponentLayerOptionType Enumeration¶
NXOpen.Assemblies.CreateNewComponentBuilder.ComponentLayerOptionType is an alias for NXOpen.Assemblies.CreateNewComponentBuilderComponentLayerOptionType
-
class
NXOpen.Assemblies.
CreateNewComponentBuilderComponentLayerOptionType
¶ Bases:
object
Set the layer option type
Enum Members
Enum Member Enum Member Description Original Set the layer option type to original Work Set the layer option type to work AsSpecified Set the layer option type to as specified -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-