CreateNewComponentBuilderComponentCamType Enumeration¶
NXOpen.Assemblies.CreateNewComponentBuilder.ComponentCamType is an alias for NXOpen.Assemblies.CreateNewComponentBuilderComponentCamType
-
class
NXOpen.Assemblies.
CreateNewComponentBuilderComponentCamType
¶ Bases:
object
Set the origin type
Enum Members
Enum Member Enum Member Description Target Set the origin type to target Resource Set the component type to resource Workpiece Set the component type to workpiece -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-