ComponentPatternCollection Class¶
-
class
NXOpen.Assemblies.
ComponentPatternCollection
¶ Bases:
object
Represents the collection object for all component patterns.
An instance of this class can be obtained from the
NXOpen.Assemblies.ComponentAssembly
.To obtain an instance of this class, refer to
NXOpen.Assemblies.ComponentAssembly
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Assemblies.ComponentPattern with the given identifier as recorded in a journal. |
GetAllComponentPatterns | Returns all the component patterns in an assembly. |
Method Detail¶
FindObject¶
-
ComponentPatternCollection.
FindObject
¶ Finds the
NXOpen.Assemblies.ComponentPattern
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Name of the component pattern to be found Returns: Component pattern with this identifier, or None if no such pattern exists Return type: NXOpen.Assemblies.ComponentPattern
New in version NX9.0.0.
License requirements: None.
GetAllComponentPatterns¶
-
ComponentPatternCollection.
GetAllComponentPatterns
¶ Returns all the component patterns in an assembly.
Signature
GetAllComponentPatterns()
Returns: Return type: list of NXOpen.Assemblies.ComponentPattern
New in version NX9.0.0.
License requirements: None.