ComponentGroupCollection Class¶
-
class
NXOpen.Assemblies.
ComponentGroupCollection
¶ Bases:
object
Contains a collection of Component Groups a
NXOpen.Assemblies.ComponentGroup
that are defined within an Assembly part.To obtain an instance of this class, refer to
NXOpen.Part
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateComponentGroup | Creates a NXOpen.Assemblies.ComponentGroup with the given name |
FindObject | Finds the NXOpen.Assemblies.ComponentGroup with the given identifier as recorded in a journal. |
Method Detail¶
CreateComponentGroup¶
-
ComponentGroupCollection.
CreateComponentGroup
¶ Creates a
NXOpen.Assemblies.ComponentGroup
with the given nameSignature
CreateComponentGroup(name)
Parameters: name (str) – Name for the ComponentGroup Returns: the ComponentGroup created Return type: NXOpen.Assemblies.ComponentGroup
New in version NX7.5.0.
License requirements: adv_assemblies (“ADVANCED ASSEMBLIES”)
FindObject¶
-
ComponentGroupCollection.
FindObject
¶ Finds the
NXOpen.Assemblies.ComponentGroup
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the ComponentGroup you want Returns: ComponentGroup with this identifier Return type: NXOpen.Assemblies.ComponentGroup
New in version NX5.0.0.
License requirements: None.