ComponentAssemblySubstitutionMode Enumeration¶
NXOpen.Assemblies.ComponentAssembly.SubstitutionMode is an alias for NXOpen.Assemblies.ComponentAssemblySubstitutionMode
-
class
NXOpen.Assemblies.
ComponentAssemblySubstitutionMode
¶ Bases:
object
Defines how a component substitution operation is performed.
Enum Members
Enum Member Enum Member Description NonAssociative The old component is deleted, and the new one is added SingleComponent An associative substitution is performed. As far as possible, this will attempt to preserve assembly constraints and interpart links. All An associative substitution is performed on all components that represent the same prototype part. This effectively substitutes one child part for a new one. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-