ComponentAssemblyOpenComponentStatus Enumeration¶
NXOpen.Assemblies.ComponentAssembly.OpenComponentStatus is an alias for NXOpen.Assemblies.ComponentAssemblyOpenComponentStatus
-
class
NXOpen.Assemblies.
ComponentAssemblyOpenComponentStatus
¶ Bases:
object
Open Component Status
Enum Members
Enum Member Enum Member Description SuccessfullyOpened The component was opened as expected DeletedByOpen The component was deleted on load as a result of the open CouldNotOpen The component could not be opened -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-