ComponentAssemblyCloseModified Enumeration¶
NXOpen.Assemblies.ComponentAssembly.CloseModified is an alias for NXOpen.Assemblies.ComponentAssemblyCloseModified
-
class
NXOpen.Assemblies.
ComponentAssemblyCloseModified
¶ Bases:
object
Indicates how close component should handle component parts when they are modified
Enum Members
Enum Member Enum Member Description False Close only unmodified parts, not modified parts True Close all parts, modified and unmodified -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-