ClearanceAnalysisBuilderClearanceZoneSource Enumeration¶
NXOpen.Assemblies.ClearanceAnalysisBuilder.ClearanceZoneSource is an alias for NXOpen.Assemblies.ClearanceAnalysisBuilderClearanceZoneSource
-
class
NXOpen.Assemblies.
ClearanceAnalysisBuilderClearanceZoneSource
¶ Bases:
object
Specify the source of the clearance zone
Enum Members
Enum Member Enum Member Description Pair Object1 Object2 Default Defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-