AssembliesParameterPropertiesBuilderArrangementOptions Enumeration¶
NXOpen.Assemblies.AssembliesParameterPropertiesBuilder.ArrangementOptions is an alias for NXOpen.Assemblies.AssembliesParameterPropertiesBuilderArrangementOptions
-
class
NXOpen.Assemblies.
AssembliesParameterPropertiesBuilderArrangementOptions
¶ Bases:
object
The positioning mixture status options
Enum Members
Enum Member Enum Member Description IndividuallyPositioned All components are varied SamePositionInAll All components are unvaried Mixed All components are neither varied nor unvaried -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-