AssembliesGeneralPropertiesBuilderHiddenOptions Enumeration¶
NXOpen.Assemblies.AssembliesGeneralPropertiesBuilder.HiddenOptions is an alias for NXOpen.Assemblies.AssembliesGeneralPropertiesBuilderHiddenOptions
-
class
NXOpen.Assemblies.
AssembliesGeneralPropertiesBuilderHiddenOptions
¶ Bases:
object
Options for managing the hidden property on the components
Enum Members
Enum Member Enum Member Description No Do not hide the objects Yes Hide the objects Mixed Objects hidden properties differ and will not change -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-