AssembliesEventTypes Enumeration¶
-
class
NXOpen.Assemblies.
AssembliesEventTypes
¶ Bases:
object
NX Event types
Enum Members
Enum Member Enum Member Description BrowserUpdate update all relations in the browser event DeselectAll deselect all that is currently selected event PartSelectAll select all parts event PartDeselectAll deselect all parts event PartSelect select specified parts event PartDeselect deselect specified parts event PartFullyLoad part fully load event PartMakeDisplayed part make displayed part event PartMakeWork part make work part event LinkedObjectSelectAll select all linked objects event LinkedObjectDeselectAll deselect all linked objects event LinkedObjectSelect select specified linked objects event LinkedObjectDeselect deselect specified linked objects event LinkedFeatureEdit linked feature edit event LinkedFeatureBreak linked feature break event LinkedFeatureAcceptBroken linked feature accept broken event Launch browser successfully launched event Exit browser exit event -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-