ArrangementsBuilder Class¶
-
class
NXOpen.Assemblies.
ArrangementsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents an arrangements builder that selects an arrangement
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
InheritArrangementFromParent | Returns or sets the inherit arrangement from parent flag |
SelectedArrangement | Returns or sets the selected arrangement |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
InheritArrangementFromParent¶
-
ArrangementsBuilder.
InheritArrangementFromParent
¶ Returns or sets the inherit arrangement from parent flag
-------------------------------------
Getter Method
Signature
InheritArrangementFromParent
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritArrangementFromParent
Parameters: inheritArrangementFromParent (bool) – New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SelectedArrangement¶
-
ArrangementsBuilder.
SelectedArrangement
¶ Returns or sets the selected arrangement
-------------------------------------
Getter Method
Signature
SelectedArrangement
Returns: Return type: NXOpen.Assemblies.Arrangement
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedArrangement
Parameters: arrangement ( NXOpen.Assemblies.Arrangement
) –New in version NX6.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
Validate¶
-
ArrangementsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.