AddComponentBuilderLocationType Enumeration¶
NXOpen.Assemblies.AddComponentBuilder.LocationType is an alias for NXOpen.Assemblies.AddComponentBuilderLocationType
-
class
NXOpen.Assemblies.
AddComponentBuilderLocationType
¶ Bases:
object
Represents initial location type that can be present during add component
Enum Members
Enum Member Enum Member Description Snap Snap as initial location type WorkPartAbsolute Absolute of work part as initial location type DisplayedPartAbsolute Absolute of displayed part as initial location type DisplayedPartWCS WCS as initial location type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-