ArcCollection Class

class NXOpen.ArcCollection

Bases: object

Represents a collection of arcs.

To obtain an instance of this class, refer to NXOpen.BasePart

New in version NX3.0.0.

Methods

Method Description
FindObject Finds the NXOpen.Arc with the given identifier as recorded in a journal.

Method Detail

FindObject

ArcCollection.FindObject

Finds the NXOpen.Arc with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Journal identifier of the arc
Returns:
Return type:NXOpen.Arc

New in version NX3.0.0.

License requirements: None.