ApparentChainingRule Class¶
-
class
NXOpen.
ApparentChainingRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects curves which appear connected or tangent connected in a particular drafting view.New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the apparent chaining rule: NXOpen.ApparentChainingRule |
Method Detail¶
Dispose¶
-
ApparentChainingRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX8.0.0.
License requirements: None.
GetData¶
-
ApparentChainingRule.
GetData
¶ Gets the data for the apparent chaining rule:
NXOpen.ApparentChainingRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (seed, view, chainingRule, selectionMask, chainingTolerance, angleTolerance) seed is a
NXOpen.ICurve
. The seed curve. view is aNXOpen.View
. The view. chainingRule is aNXOpen.ApparentChainingRuleType
. Selection Intent method, either of Connected Curves, Tangent Curves or Single Curve. selectionMask is aNXOpen.ApparentChainingRuleSelection
. The selection type none, edge or curve. chainingTolerance is a float. Gap toleranceangleTolerance is a float. Angle tolerance .. versionadded:: NX8.0.0License requirements: gateway (“UG GATEWAY”)