ZeroToleranceDisplayStyle Enumeration¶
-
class
NXOpen.Annotations.
ZeroToleranceDisplayStyle
¶ Bases:
object
Specifies the 0 tolerance display style Enum Members
Enum Member Enum Member Description BasedOnUnits Zero tolerance display is tied to display units AsZero Always display zero tolerance as 0 OmittedAndInlined Omit the display of zero tolerance and inline the remaining tolerance Omitted Omit the display of zero tolerance and maintain position of remaining tolerance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-