TolerancePlacement Enumeration¶
-
class
NXOpen.Annotations.
TolerancePlacement
¶ Bases:
object
Specifies the tolerance text placement relative to the dimension text Enum Members
Enum Member Enum Member Description Below Specifies tolerance below dimension text After Specifies tolerance after dimension text Above Specifies tolerance above dimension text Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-