TitleBlockCellBuilder Class¶
-
class
NXOpen.Annotations.
TitleBlockCellBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.TitleBlockCellBuilder
To create a new instance of this class, use
NXOpen.Annotations.TitleBlockCollection.CreateCellBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Cell | Returns the tabular note cell corresponding to this title block cell |
EditableText | Returns or sets the editable text of the cell |
Label | Returns or sets the cell label |
Lock | Returns or sets the lock status |
Tag | Returns the Tag for this object. |
Text | Returns the evaluated text of the cell. |
Methods¶
Method | Description |
---|---|
EditCell | Edits the title block cell attributes such as lock status, content type, value, label etc. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Cell¶
-
TitleBlockCellBuilder.
Cell
¶ Returns the tabular note cell corresponding to this title block cell
-------------------------------------
Getter Method
Signature
Cell
Returns: The tabular note cell corresponding to this title block cell Return type: NXOpen.DisplayableObject
New in version NX10.0.2.
License requirements: None.
EditableText¶
-
TitleBlockCellBuilder.
EditableText
¶ Returns or sets the editable text of the cell
-------------------------------------
Getter Method
Signature
EditableText
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EditableText
Parameters: text (str) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Label¶
-
TitleBlockCellBuilder.
Label
¶ Returns or sets the cell label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (str) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Lock¶
-
TitleBlockCellBuilder.
Lock
¶ Returns or sets the lock status
-------------------------------------
Getter Method
Signature
Lock
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Lock
Parameters: lockStatus (bool) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
EditCell¶
-
TitleBlockCellBuilder.
EditCell
¶ Edits the title block cell attributes such as lock status, content type, value, label etc.
Signature
EditCell(lockStatus, contentType, value, label, canChangeLockStatus)
Parameters: - lockStatus (bool) – cell lock status
- contentType (int) – cell content type
- value (str) – cell value
- label (str) – cell label
- canChangeLockStatus (bool) – can change lock status of cell
New in version NX10.0.2.
License requirements: drafting (“DRAFTING”)
Validate¶
-
TitleBlockCellBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.