TextWithSymbolsBuilderSymbolSizingMethod Enumeration¶
NXOpen.Annotations.TextWithSymbolsBuilder.SymbolSizingMethod is an alias for NXOpen.Annotations.TextWithSymbolsBuilderSymbolSizingMethod
-
class
NXOpen.Annotations.
TextWithSymbolsBuilderSymbolSizingMethod
¶ Bases:
object
sizing method for embedded user-defined symbols
Enum Members
Enum Member Enum Member Description ScaleAndAspectRatio Size using scale and aspect ratio LengthAndHeight Size using length and height -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-