TextWithSymbolsBuilderSymbolPreferencesType Enumeration¶
NXOpen.Annotations.TextWithSymbolsBuilder.SymbolPreferencesType is an alias for NXOpen.Annotations.TextWithSymbolsBuilderSymbolPreferencesType
-
class
NXOpen.Annotations.
TextWithSymbolsBuilderSymbolPreferencesType
¶ Bases:
object
Enum for the symbol preferences
Enum Members
Enum Member Enum Member Description UseCurrent Use Current UseDefinition Use Definition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-