TextPreferencesOption Enumeration¶
-
class
NXOpen.Annotations.
TextPreferencesOption
¶ Bases:
object
Specifies the custom symbol text preferences option. This option is only available when creating. Enum Members
Enum Member Enum Member Description PartLettering Specifies current part files’s lettering preferences will be used MasterSymbol Specifies master symbol’s text preferences will be used Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-