TextPlacement Enumeration¶
-
class
NXOpen.Annotations.
TextPlacement
¶ Bases:
object
Specifies the dimension text placement Enum Members
Enum Member Enum Member Description Automatic Specifies automatic text placement ManualArrowsIn Specifies manual text placement with arrows inside the extension lines ManualArrowsOut Specifies manual text placement with arrows outside the extension lines ManualArrowsInSameDirection Specifies manual text placement with arrows in the same direction Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-