TextOrientation Enumeration¶
-
class
NXOpen.Annotations.
TextOrientation
¶ Bases:
object
Specifies the dimension text orientation Enum Members
Enum Member Enum Member Description Horizontal Specifies horizontal dimension text Aligned Specifies dimenson text aligned with the dimension line OverDimensionLine Specifies dimenson text aligned with and above the dimension line ByAngle Specifies dimension text at angle Perpendicular Specifies dimension text perpendicular to the dimension line SplitByDimensionLine Specifies dimenson text split by the dimension line Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-