TextJustification Enumeration

class NXOpen.Annotations.TextJustification

Bases: object

Represents the horizontal text justification Enum Members

Enum Member Enum Member Description
Left
Center
Right
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.