TextComponentTextType Enumeration¶
NXOpen.Annotations.TextComponent.TextType is an alias for NXOpen.Annotations.TextComponentTextType
-
class
NXOpen.Annotations.
TextComponentTextType
¶ Bases:
object
the text type.
Enum Members
Enum Member Enum Member Description Text primary dimension text or main text for draft aids DualDimension dual dimension text Tolerance tolerance text DualTolerance dual tolerance text DiameterRadius diameter or radius or arc length symbol text AppendedAbove appended text above AppendedBelow appended text below AppendedBefore appended text before AppendedAfter appended text after ChamferBefore chamfer text before ChamferAfter chamfer text after ChamferSize chamfer size text ChamferXSymbol chamfer x symbol text ChamferAngle chamfer angle symbol text -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-