TargetPointCollection Class¶
-
class
NXOpen.Annotations.
TargetPointCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.TargetPoint
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateTargetPointBuilder | Creates the TargetPointBuilder |
FindObject | Finds the target point with the given name. |
Method Detail¶
CreateTargetPointBuilder¶
-
TargetPointCollection.
CreateTargetPointBuilder
¶ Creates the TargetPointBuilder
Signature
CreateTargetPointBuilder(targetPt)
Parameters: targetPt ( NXOpen.Annotations.TargetPoint
) –NXOpen.Annotations.TargetPoint
to be edited, if None then create a new oneReturns: TargetPointBuilder object Return type: NXOpen.Annotations.TargetPointBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FindObject¶
-
TargetPointCollection.
FindObject
¶ Finds the target point with the given name.
An exception will be thrown if no object can be found with given name
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the target point to be found Returns: Target Point with this identifier Return type: NXOpen.Annotations.TargetPoint
New in version NX6.0.0.
License requirements: None.