TableColumnBuilderScopeType Enumeration

NXOpen.Annotations.TableColumnBuilder.ScopeType is an alias for NXOpen.Annotations.TableColumnBuilderScopeType

class NXOpen.Annotations.TableColumnBuilderScopeType

Bases: object

The options determine whether to apply settings to all cells or only to cells of new rows.

Enum Members

Enum Member Enum Member Description
CellsinNewRows
AllCellsinColumn
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.