TableColumnBuilderCategoryType Enumeration

NXOpen.Annotations.TableColumnBuilder.CategoryType is an alias for NXOpen.Annotations.TableColumnBuilderCategoryType

class NXOpen.Annotations.TableColumnBuilderCategoryType

Bases: object

The options specify the type of column.

Enum Members

Enum Member Enum Member Description
General
Callout
Quantity
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.