TableCellStyleBuilderZeroDisplayType Enumeration

NXOpen.Annotations.TableCellStyleBuilder.ZeroDisplayType is an alias for NXOpen.Annotations.TableCellStyleBuilderZeroDisplayType

class NXOpen.Annotations.TableCellStyleBuilderZeroDisplayType

Bases: object

the valid zero display types

Enum Members

Enum Member Enum Member Description
Zero
Dash
Empty
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.