TableCellStyleBuilderTimeFormatTypes Enumeration¶
NXOpen.Annotations.TableCellStyleBuilder.TimeFormatTypes is an alias for NXOpen.Annotations.TableCellStyleBuilderTimeFormatTypes
-
class
NXOpen.Annotations.
TableCellStyleBuilderTimeFormatTypes
¶ Bases:
object
the time format types
Enum Members
Enum Member Enum Member Description Hhmm24 24 hh:mm Hhmm12 12 hh:mm AM/PM Hhmmss24 24 hh:mm:ss Hhmmss12 12 hh:mm:ss AM/PM -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-