TableCellStyleBuilderDateFormatTypes Enumeration

NXOpen.Annotations.TableCellStyleBuilder.DateFormatTypes is an alias for NXOpen.Annotations.TableCellStyleBuilderDateFormatTypes

class NXOpen.Annotations.TableCellStyleBuilderDateFormatTypes

Bases: object

the date format types

Enum Members

Enum Member Enum Member Description
Ddmmmyyyy
Ddmmm
Mmmyyyy
Mmddyyyy
Yymmmdd
Yyyymmdd
Ddmmyyyy
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.