TableCellStyleBuilderCellFormatTypes Enumeration¶
NXOpen.Annotations.TableCellStyleBuilder.CellFormatTypes is an alias for NXOpen.Annotations.TableCellStyleBuilderCellFormatTypes
-
class
NXOpen.Annotations.
TableCellStyleBuilderCellFormatTypes
¶ Bases:
object
the cell format types
Enum Members
Enum Member Enum Member Description Text Text Float Float Fixed Fixed General General Monetary Monetary Comma Comma FractionHalfSize Fraction half size FractionThreeQuarterSize Fraction three quarter size FractionFullSize Fraction full size DegreesDegreeUnits Degrees DegreesRadianUnits Radians Percent Percent Degrees Radians Hex Hex Logic Logic Hidden Hidden Custom Custom Date Date Time Time DateTime Date-Time -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-