SurfaceFinishStandard Enumeration¶
-
class
NXOpen.Annotations.
SurfaceFinishStandard
¶ Bases:
object
Specifies the drafting surface finish standard type Enum Members
Enum Member Enum Member Description Ansi ANSI Iso ISO Jis JIS Din DIN Iso2002 ISO 2002 Din2002 DIN 2002 Gb GB131-93 Eskd ESKD -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-