SuppressPMIBuilderSuppressionMethodType Enumeration¶
NXOpen.Annotations.SuppressPMIBuilder.SuppressionMethodType is an alias for NXOpen.Annotations.SuppressPMIBuilderSuppressionMethodType
-
class
NXOpen.Annotations.
SuppressPMIBuilderSuppressionMethodType
¶ Bases:
object
Suppression methods
Enum Members
Enum Member Enum Member Description NotSet Unsuppress selected PMI objects. Manual Suppress selected PMI objects. CreateExpressionForEach Creates expressions for controlling the suppression of each selected PMI object. CreateSharedExpression Creates a single expression for controlling the suppression of the selected PMI objects and suppresses them. SelectExpression Allows selection of an expression to control the suppression of the selected PMI objects. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-